Install FT Service Platform

NOTE:
If FT Service Platform is already installed, user must apply the FTSP patch. Refer to KB RAID 1092336: https://rockwellautomation.custhelp.com/app/answers/detail/a_id/1092336
To connect InfoPlatform with FactoryTalk Live Data or Historian install the following:
  • Before installing, check if the FactoryTalk Service Platform is already installed on the computer.
  • To install the service platform, run the setup from the media as specified in the section.
  • To confirm installation, launch Windows Control Panel and select the Programs applet.
    Verify Installation
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal