View Installation Log
If the installation is performed using the log switch command (see “FTAnalytics InfoPlatform Installation”), User can view log information generated during the installation in the file specified in the command.
Provide Feedback