Transport Layer Security (TLS)
InfoPlatform can be easily configured to run over HTTPS using TLS. Similarly, SignalR can be configured to run over WSS, both requiring digitally signed certificates to secure the communication between the client and the server. This section describes the configuration steps when securing the service.
Provide Feedback