Supported Platforms

Operating system
Supported Editions
Windows Server 2019
64-bit
Windows Server, version 1803
64-bit
Windows Server 2016
64-bit
Windows Server 2012 R2
64-bit
Windows Server 2012 (64-bit edition)
64-bit
Windows Server 2008 R2 SP1
64-bit
These requirements are for the InfoPlatform service on its own. Additional H/W restrictions may exist for other components such as FTHistorian. Refer to the product documentation of those components for their requirements.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal