Certificate Validation Option

When configuring the OPC UA provider in the InfoPlatform configuration file (see Enable the OPC UA connector for more details). User can stipulate certificate validation options for certified connections being made to the server. Possible options are as shown below. Depending on the option selected, the certificate will be kept in a permanent store, a rejected store, or accepted temporarily.
Property Name
Description
Reject
Reject the certificate.
AcceptOnce
Accept the certificate temporarily.
AcceptAlways
Accept the certificate always.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal