InfluxDB

NOTE:
In the application, this InfluxDB is also called as InfluxDB1 (Version 1) connected to FactoryTalk Service.
InfluxDB is designed to work with time-series data. In short, InfluxDB is made to store a large volume of time-series data and perform real-time analysis on those data, quickly. In InfluxDB, a timestamp identifies a single point in any given data series. This is like an SQL database table where the primary key is pre-set by the system and is always time. See the online documentation for more details.
InfluxDB
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal