InfluxDB Model

The InfluxDB server model contains:
  • Databases
    : A logical container for users, retention policies, continuous queries, and time series data.
  • Measurements
    : The part of InfluxDB’s structure that describes the data stored in the associated fields.
  • Fields
    : The key-value pair in InfluxDB’s data structure that records metadata and the actual data value. Fields are required in InfluxDB’s data structure and they are not indexed.
  • Tags
    : The key-value pair in InfluxDB’s data structure that records metadata. Tags are an optional part of InfluxDB’s data structure but they are useful for storing commonly-queried metadata; tags are indexed so queries on tags are performant.
Here is a typical InfluxDB model:
InfluxDB - Fields
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal