Configure FTEGInfluxDB in FTA InfoPlatform Service

To enable the connector, user has to add the following XML structure to the "FactoryTalk Analytics InfoPlatform Service" configuration file ("RA.InfoPlatform.WindowsService.exe.config").
<PlugIns> <add assembly="RA.InfoPlatform.InfluxDB2Provider" type="RA.InfoPlatform.InfluxDB2Provider.PlugIn"> <Parameters> <add name="ConfigFile" value="InfluxDB2-Plugin.config" /> </Parameters> </add> </PlugIns>
With three parameters user can specify the behavior of the connector:
Property Name
Description
ConfigFile
Defines the file that should be used to configure the InfluxDB server connections.
  • Define a Connection to FTEGInfluxDB Server
    All FTEGInfluxDB connections are defined in the InfluxDB2-Plugin.config configuration file (JSON format). For connecting to FTEGInfluxDB datasource, user should provide connection string into InfluxDB2-plugin.config. For example:
    [ { "InstanceName": "InfluxDB2-Server-1", "ServerUrl": "http://<hostname>:8086", "Authorization": "7GIJDEWHZoLwfGpXEqYxxrg3O2TmxoXFVDsjfh_QA4OBpQgwiK6ZPM1vDPv2e-2E7cgkOEBdkERBOW bhLhMwVw==", "BucketName": “Demobucket”, "PasswordEncrypted": false } ]
Property Name
Description
InstanceName
This will be unique instance name of Connection
ServerUrl
Provide InfluxDB2 server URL with port based on the configuration.
http://<hostname>:<port>
Authorization
It will hold Token code with all privilleges (must) to access the Bucket.
BucketName
This will hold specific bucket name to map into database and display in navigation. Mapped database name will be same as bucket name.
PasswordEncrypt ed
Default value will be false. Token code will be encrypted after service restart
  • Restart InfoPlatform service.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal