Verify HTTPS Configuration
- Log in to DataView application, under the Connection tab, click [Add Connections].
- Select [FactoryTalk Service] under the Rockwell Automation drop-down list.
- Provide the parameters and click [Test Connection]. If all the details are valid, the “Test connection successful” message displays.NOTE:Username and Password are required if FTASecurity is enabled.Test Connection
- Verify the InfoPlatform tags available under FactoryTalk Service model.InfoPlatform Tags
Provide Feedback