Simulator

In addition to Historians, the InfoPlatform service includes a
Simulator
data provider that can be useful for development or debugging purposes.
The following entry in the config file must be included for the simulator data provider to be enabled:
<add assembly="RA.InfoPlatform.Connector.Simulator.MiddleTier" type="RA.InfoPlatform.Connector.Simulator.MiddleTier.PlugInInfo" />
The diagram below shows a sample representation of the name space including the Simulator.
Tags
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal