Reports tab

How do I open the Reports tab?
  1. Select Settings button.
  2. Select the
    Reports
    tab.
Use the
Reports
tab to configure the automatic saving settings for reports of each flash operation, including:
  • Option to turn on or off the automatic saving.
  • Location of the saved report.
With the
Save a report for each flash operation automatically
checkbox selected, a report summarizing the flash result is automatically saved when a flash operation completes.
To change the report location, click
Change
. The default location is C:\Users\<Username>\Documents\ControlFLASH Plus\Reports.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal