Enable application log

When an application error occurred during operations, view the application log to check the causes of the error.
Prerequisites
  • In
    Settings > General
    , select
    Enable application log for troubleshooting
    and restart
    ControlFLASH Plus
    .
To enable application log
  1. In the
    ControlFLASH Plus
    window, select Settings button.
  2. In the
    Settings
    dialog box, select the
    General
    tab.
  3. On the
    General
    tab, select the
    Enable application log for troubleshooting
    checkbox.
    The default path for application logs shows and you are prompted with a dialog box indicating that when launching
    ControlFLASH Plus
    next time, application logging will begin.
  4. Select
    Close
    .
    TIP:
    The application logs will be created on application start and stopped at application stop. Select the path link to open the default folder for application logs.
  5. Select
    OK
    .
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal