Firmware Locations tab
How do I open the Firmware Locations tab?
- Select
.
- Select theFirmware Locationstab.
Use the
Firmware Locations
tab to view and manage the file locations that ControlFLASH Plus
monitors for revision files.- To add a monitored location, clickAdd Location, select the target folder, and then clickOK. ClickOKin theSettingsdialog box to save the change.TIP:If you use the download manager to download firmware revisions from the Product Compatibility and Download Center, the default or customized path of the firmware revisions will be added to the location list automatically.
- To set a default monitored location, click
at the end of the location. Select
Set as download location, and then clickOKin theSettingsdialog box to save the change. - To remove a monitored location, in the location list, click
at the end of the location. Select
Remove, and then clickOKin theSettingsdialog box to save the change. - To open a monitored download location, click the location in the location list.TIP:
- Once a monitored download location is set as default, its
is disabled.
- The following locations are listed by default and cannot be removed:
- C:\Program Files (x86)\ControlFLASH
- C:\Users\<Username>\Downloads\RA
- C:\Users\Public\Documents\Rockwell Automation\Firmware Kits
Provide Feedback