Export firmware inventory

Export the firmware inventory to create a backup for the firmware revisions' information.
To export the firmware inventory
  1. On the Manage Firmware tab, select Export Revisions button.
  2. In the
    Save As
    dialog box, select a path and enter a name for the exported file.
  3. Select
    Save
    .
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal