Delete firmware revisions

Delete one or multiple unused firmware revisions in a single operation to improve inventory building performance.
Prerequisites
  • Make sure the currently signed in user has permission to delete firmware revisions.
To delete firmware revisions
  1. On the Manage Firmware tab, select Delete Revisions to turn on the delete mode.
  2. Select the checkboxes of firmware revisions that you want to delete.
    TIP:
    Select a device's checkbox to select all its firmware revisions. If you don't select all the firmware revisions of a device, the checkbox will appear dimmed.
  3. Select
    Delete
    .
    The
    Delete
    button appears dimmed when updating devices or downloading firmware revisions.
  4. When prompts, confirm the firmware revisions list.
  5. Select
    Delete
    .
    If the deletion fails, check the permissions of the firmware.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal