Add Firmware Revisions
After signing in to the Product Compatibility and Download Center, use the
Add Revisions
dialog box to download firmware revisions and view firmware revisions' Important Notice.Prerequisites
To add firmware revisions
- In the Add Firmware Revisions dialog box, search devices, and then select firmware revisions as needed.
- (optional) Select
to view the firmware revisions' Release Notes or select
to view the firmware revisions' Important Notice.
- (optional) SelectView selected revisionsto view the firmware revisions you select.
- SelectDownload.TIP:When the operation completes:
- If it is a DMK file, the revision will appear in theRevisionscolumn automatically.
- If it is a non-DMK file, selectNon-DMK firmware must be installed manuallyto locate the firmware in the monitored folder, and then install the firmware manually. The revision will appear in theRevisionscolumn after refreshing the firmware.
Provide Feedback