Rename a favorite list
Change a name of a favorite list for easy recognition. This can be helpful especially when using the
Flash Devices
tab to create favorite lists, in which case the first created one is named Favorites
while subsequent ones have a number appended to the name.To rename a favorite list
- On theManage Favoritestab, double-click the name of a favorite list.
- Enter the name of the favorite list.
- PressEnteror click anywhere outside the name box to save the change.
Provide Feedback