Export all the favorite lists

Export all the favorite lists as a CFF file so that you can easily share with others, or for example, save a backup copy.
To export all the favorite lists
  1. On the
    Manage Favorites
    tab, click
    Export all
    .
  2. In the
    Save As
    dialog box, name the CFF file and select a location to save it.
  3. Click
    Save
    .
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal