Create a favorite list
Create a favorite list to include devices and associated revisions. When flashing devices, use the favorite list to quickly select devices and revisions to your liking. A favorite list can be created on the
Flash Devices
tab or the Manage Favorites
tab.To create a favorite list on the Flash Devices tab
- Select the devices to include in the favorite list.
- In theFlash Tocolumn, select the revision to flash to.TIP:Make sure to select the same revision for each selected device type.
- ClickCreate Favorite List.TheManage Favoritestab shows and the favorite list is added toFavorite Lists.
To create a favorite list on the Manage Favorites tab
- In theNew Favorite Listbox, enter the name of the favorite list.
- PressEnter.
- In theSearch devicestext box of theAdd Devicesdialog box, enter the name of the device to include in the favorite list.
- Select the checkbox of the device and its associated revision.TIP:ClickView selected devicesto view only the selected devices and revisions.
- ClickAdd.
Provide Feedback