Add devices to a favorite list
Select devices available from the monitored folders and add them to an existing favorite list.
To add devices to a favorite list
- On theManage Favoritestab, select a favorite list.
- ClickAdd devices.
- In theSearch devicestext box of theAdd Devicesdialog box, enter the name of the device to include in the favorite list.
- Select the checkbox of the device and its associated revision.TIP:ClickView selected devicesto view only the selected devices and revisions.
- ClickAdd.
Provide Feedback