View a flash report

Once a flash operation completes, you can view the CSV report file summarizing the result of the operation.
To view a flash report
  1. After a flash operation completes, click
    Close
    when you are prompted with the
    Flash Results
    dialog box.
  2. If auto-save is off, click
    Create Report
    .
    If auto-save is on, go to step 5.
  3. In the
    Save as
    dialog box, navigate to the location used to save the report.
    TIP:
    The default name of the report follows the format as
    ControlFLASH Plus Report <year_month_day_hour_minute_second>.
  4. Click
    Save
    .
  5. Click
    Show Reports
    .
  6. Double-click the report to open it.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal