Flash operation statuses

The following table lists the statuses of flash operations and their meanings.
Status
Description
Flash finished
A device is flashed successfully.
Failed
A device is not flashed successfully.
Transmitting update
A device is being flashed.
Polling for power-up
ControlFLASH Plus
is waiting for the device to power up.
Pending
The flashing of the device is queued to start later in the flashing schedule.
Flash interrupted
An interruption occurs to a flash operation.
Canceled
A flash operation is canceled.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal