Fix interrupted flash operations

When an interruption happens during a flash operation for the selected devices, you have to take actions. The interruption status and the number of interrupted flashes show at the top of the
Flash Devices
tab.
To fix interrupted flash operations
  1. At the top of the
    Flash Devices
    tab, click
    View
    .
  2. In the
    Status
    column of an interrupted device, click
    Resolve
    .
    TIP:
    When
    ControlFLASH Plus
    does not have focus, an interrupted flash operation will cause
    ControlFLASH Plus
    icon to flash in the taskbar.
  3. Read the information and follow the instructions in the
    Flash interrupted
    dialog box.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal