Download operation statuses
The following table lists the download operation statuses and their meanings.
Status | Description |
---|---|
Pending | A firmware revision is waiting to be downloaded and ![]() |
Downloading | A firmware revision is being downloading and ![]() |
Loading | ControlFLASH Plus is loading the firmware revisions after download completes. The Next button becomes available when loading finishes. |
Non-DMK firmware must be installed manually | The downloaded file is a non-DMK file. Select the link to locate the file in the download folder, and then install the firmware revision manually. Refreshing firmware is required after installing non-DMK firmware kits. |
Unable to download | The firmware revision download fails. Select ![]() |
Unable to flash device to this revision | The downloaded firmware revision is not compatible with this device's hardware series. Choose a firmware revision that is compatible. |
Provide Feedback