Download Center License Agreement

The following table lists the options in the
Download Center License Agreement
dialog box and their meanings.
Option
Description
Language
Selects the language of the agreement from the Product and Compatibility and Download Center. The default language is English.
Accept
Selects this button to start the download.
Decline
Selects this button to cancel the download.
Unable to download revision
shows in the
Status
column.
Tip
: Select
Next
to continue flashing the devices with local firmware revisions.
Cancel
Selects this button to return to the start page.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal