Components

The following table explains the items in the
Compatibility
dialog box and their meanings.
Item
Description
Lock Revision
This column shows the current device's locked or unlocked status. Hover over the blank cell and click Lock icon to lock the current device revision. The unlocked devices' compatible choices will be updated to ensure the compatibility with the locked device revision.
Lock one or multiple devices as needed.
Unlock the locked devices if there are no compatible firmware revisions.
Current Choices
This column shows the following subcolumns:
  • Device
    shows devices with compatibility issues.
  • In Device
    shows each device's current firmware revision.
  • Flash To
    shows each device's firmware revision selected on the
    Flash Devices
    tab.
Compatible Choices
This column shows suggested compatible firmware revisions.
  • Closest Compatible
    shows all compatible firmware revisions that are closest to the current firmware revisions.
    Note
    : The closest compatible firmware revision won't be lower than the selected revision.
  • Latest Compatible
    shows all compatible firmware revisions that are latest from the Product Compatibility and Download Center.
Indications appear if there are locked devices and no compatible firmware revisions.
Ignore incompatible firmware revisions
This column shows the delete icons. Click Close icon to ignore the current incompatible device. Ignored devices will be removed from this dialog box and still listed on the
Flash Devices
tab.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal