The co-existence of ControlFLASH and ControlFLASH Plus
- ControlFLASHandControlFLASH Pluscan be installed and run on the same computer.
- ControlFLASHandControlFLASH Plusshare the same product policy setting inFactoryTalk Administration Console, that is,ControlFlash.
- UninstallingControlFLASHwill cause legacy MSI firmware kits to become inaccessible toControlFLASH Plus. To recover legacy firmware kits that have become inaccessible toControlFLASH Plus, simply install the latest version ofControlFLASH.
Provide Feedback