Configure ControlFLASH Plus policy

In case you need to configure security policies for
ControlFLASH Plus
, use the following steps to do so.
To configure
ControlFLASH Plus
policy
  1. Open FactoryTalk Administration Console.
  2. In the
    Select FactoryTalk Directory
    dialog box, select
    Network
    , and then click
    OK
    .
  3. In
    Explorer
    , expand
    System > Policies > Product Policies > ControlFlash
    and double-click
    Feature Security
    .
    TIP:
    ControlFLASH Plus
    and
    ControlFLASH
    use the same product policy settings.
  4. In the
    Feature Security Properties
    dialog box, click Browse next to
    Firmware: Update
    .
  5. In the
    Configure Securable Action
    dialog box, view or configure permissions for a user or group.
  6. Click
    OK
    .
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal