Overview view parameters

The
Overview
view includes these parameters.
Definition
Parameter
Description
Vendor
Displays the device manufacturer information.
Product type
Displays the type and description of the device being configured.
Product code
Displays the product code of the device.
Revision
Displays the device major and minor revisions.
Electronic keying
Displays the electronic keying used for the device. Electronic keying compares the device defined in the project to the installed device. If keying fails, a fault occurs.
Valid values include:
  • Exact Match
  • Compatible Module
  • Disable Keying
For detailed information on Electronic keying, see Electronic Keying in Logix5000 Control Systems Application Technique, publication LOGIX-AT001.
Connection
Displays the connection type as
Data
,
Input Data
,
Data with Status
, or
Input Data with Status
.
Data Format
Displays the type of data transferred between the device and the parent. Valid values include:
  • INT (16-Bit)
  • SINT (8-Bit)
  • DINT (32-Bit)
  • DINT (32-Bit) - Small Config
  • REAL (32-Bit)
Connections
Parameter
Description
Connection
Displays the connection type as
Standard
or
Status
.
Input Assembly Instance
Displays the input connection point for the standard input connection. The default value is 1.
Input Size
Displays the size of the input assembly.
Input Size Unit
Displays the unit of the Input Size value.
Output Assembly Instance
Displays the output connection point for the standard output connection. The default value is 2.
Output Size
Displays the size of the output assembly.
Output Size Unit
Displays the unit of the Output Size value.
Configuration Assembly Instance
Displays the target of the connection. The default value is 199.
Configuration Size
Displays the size of the configuration assembly.
Configuration Size Unit
Displays the unit of the Configuration Size value.
Others
Parameter
Description
Device definition
Opens the dialog box to change the device definition or the connection configuration.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal