Windows view parameters
The
Windows
view includes these parameters:
TIP:
These parameters are not available in Run mode.
Parameter | Description |
|---|---|
Window | Indicates the window to which the configuration applies. |
Output On Value | The On Value for Window 1 is disabled and set to 0 when the counter type is Pulse Width Modulation (PWM). When the counter type is Period/Rate, Continuous/Rate, Rate Measurement, or Pulse Generator (for Windows 1…4), the valid range is 0…16,777,215. When the counter type is Counter, Encoder X1, Encoder X2, Encoder X4, or Pulse Generator, for Windows 1…4, the valid values are less than or equal to the Rollover value. When tied to the compare dialog, Outputs 0 and 1 are selected. The On Value must not equal 0. The On Value must be different from the Off Value. You have the option to set the On Value for Windows to zero if outputs are not tied to the compare dialog. |
Output Off Value | The Off Value for Window 1 is disabled and set to 0 when the counter type is Pulse Width Modulation (PWM). When the counter type is Period/Rate, Continuous/Rate, Rate Measurement, or Pulse Generator (for Windows 1…4), the valid range is 0…16,777,215. When the counter type is Counter, Encoder X1, Encoder X2, Encoder X4, or Pulse Generator, for Windows 1…4, the valid values are less than or equal to the Rollover value. When tied to the compare dialog, Outputs 0 and 1 are selected. The Off Value must not equal 0. The Off Value must be different from the On Value. You have the option to set the Off Value for Windows to zero if outputs are not tied to the compare dialog. |
Output 0 | Ties Output 0 of the VHSC device to the corresponding Window. Output 0, by default, is not tied to any Windows. |
Output 1 | Ties Output 1 of the VHSC device to the corresponding Window. Output 1, by default, is not tied to any Windows. |
Provide Feedback