Points view parameters
The
Points
view includes these parameters:
TIP:
These parameters are not available in Run mode.
Parameter | Description |
|---|---|
Point | Configures the parameters for the specified point. |
Input Filter Time | Sets a time by which to delay the transition from Off to On or from On to Off. This feature is useful for filtering out transients in noisy environments. Select a value in milliseconds (ms). The valid range is from 0.000 through 65.535. The default value is 1.000. |
Open Wire | Configures the Open Wire Enable and Disable bit for all points. A check mark indicates that open wire is enabled. The checkbox is selected by default.
|
Provide Feedback