Device definition dialog box parameters
Parameter | Description |
|---|---|
Device type | Displays the device catalog number and type. |
Name | Specifies the device name. The name must be IEC_61131 compliant. If an invalid character is entered in this
field or if the name exceeds 40 characters, the software ignores the character. |
Description | Specifies the description for the device. The description must be within 512 characters. If the description exceeds the
maximum length, the software ignores any extra characters. |
Chassis size | Sets the chassis size. Only valid sizes are available. |
Slot | Specifies the slot number where the device resides from 0 through the maximum
number of devices determined by the selected chassis size minus 1. |
Revision | Specifies the major and minor revisions of the device. The valid range for minor
revision is from 1 through 255. |
Electronic keying | Defines the electronic keying used for the device. Electronic keying compares the
device defined in the project to the installed device. If keying fails, a fault
occurs. Valid values include:
For detailed information on Electronic keying, see Electronic Keying in Logix5000 Control Systems
Application Technique, publication LOGIX-AT001. |
Ethernet address | Specifies the IP configuration for the device. Possible options include:
|
Provide Feedback