Alarms view

Use
Alarms
to define limits. Use this view to:
  • Set the high and low limits of position alarm counts.
  • Set the high limit, low limit, and hysteresis of velocity.
  • Set the high limit, low limit, and hysteresis of acceleration.
  • Set the units, high limit, and low limit of temperature.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal