Alarms view
Use
Alarms
to define limits and:- Set the high and low limits of position alarm counts.
- Set the high limit, low limit, and hysteresis of velocity.
- Set the high limit, low limit, and hysteresis of acceleration.
- Set the units, high limit, and low limit of temperature.
Provide Feedback