Channel values too close

One or more of these scenarios may be true:
  • Low Engineering and High Engineering values are equal.
  • High Signal value is less than Low Signal value.
  • Low Signal and High Signal values are equal.
Check the configuration, make the required modifications, and apply the changes.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal