Configure output parameters
Configure output parameters for the high-speed counter device.
To configure output parameters
- On the tab for the device, selectOutputs.
- In theOutputsview, fill in the parameters and selectOK.
Provide Feedback