Events view parameters

The
Events
view includes these parameters:
Parameter
Description
Member Name
Value
Event
The event number to which this configuration applies.
Enable Event
Determines whether the corresponding event trigger is active. Events are triggered once conditions match the definition.
EO.Event0x.En
0 = Event trigger definition is not active
1 = Event trigger definition is active
Latch Event
Determines what happens to the current event when a new event is received. When this parameter is selected, events are latched until acknowledged. A new event is lost if the previous event was not acknowledged. When this parameter is not selected, new events overwrite old events.
EO.Event0x.LatchEn
0 = Event is not latched. New events overwrite old events.
1 = Event is latched. New events are lost if the latched event was not acknowledged.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal