Device definition - Counters view parameters
The
Counters
view in Device definition
includes these parameters.Parameter | Description |
|---|---|
Mode | Defines the operating mode of the counter. There are two counters. Available options are:
|
Z Terminal Function | Defines the terminal function that is used with the counter mode. Available options are:
|
Provide Feedback