Counter0x - Alarms view parameters
The
Alarms
view includes these parameters:Parameter | Description | Member Name | Value |
|---|---|---|---|
Pulse Width Alarm Limit | Specifies the maximum pulse width (C.Counter0x.PulseWidthAlarmLimit) allowed before the pulse width alarm is triggered. If the instantaneous or average pulse width (I.Counter0x.PulseWidthAvg) exceeds the maximum pulse width, the pulse width alarm is triggered. | C.Counter0x.PulseWidthAlarmLimit | Any valid floating point number |
Accel Alarm Limit | Specifies the maximum acceleration rate (C.Counter0x.AccelAlarmLimit) allowed before the acceleration alarm is triggered. If the instantaneous or average acceleration rate (I.Counter0x.AccelAvg) exceeds the maximum acceleration rate, the acceleration alarm is triggered. | C.Counter0x.AccelAlarmLimit | Any non-negative floating point value |
Decel Alarm Limit | Specifies the maximum deceleration rate allowed before the deceleration alarm is triggered. If the instantaneous or average acceleration rate is less than the maximum deceleration rate, the deceleration alarm is triggered. | C.Counter0x.DecelAlarmLimit | Any negative value |
Frequency Alarm Limit | Specifies the frequency allowed before the frequency alarm is triggered. If the instantaneous or average frequency exceeds this limit, the frequency alarm is triggered. | C.Counter0x.FrequencyAlarmLimit | Any positive value |
Zero Frequency Alarm Limit | Shows the value that frequency or average frequency must be less than to trigger the zero frequency alarm. | O.Counter0x.ZeroFrequencyAlarmLimit | Any |
Latch Zero Frequency Alarm | Determines whether the zero frequency alarm latches so that it does not clear until explicitly unlatched. | C.Counter0x.ZeroFrequencyAlarmLatchEn |
|
Enable Missing Pulse Alarm | Determines whether the missing pulse alarm is enabled. | O.Counter0x.MissingPulseAlarmEn |
|
Missing Pulse Alarm Limit | Shows the length of time that must elapse between detecting the leading edge of consecutive pulses (I.Counter0x.InputPulseAlarm) before the missing pulse alarm is triggered. | O.Counter0x.MissingPulseAlarmLimit | 1 to 10,000,000 (micro seconds) |
Latch Missing Pulse Alarm | Determines whether the missing pulse alarm latches so that it does not clear until explicitly unlatched (O.Counter0x.MissingPulseAlarmUnlatch). | C.Counter0x.MissingPulseAlarmLatchEn |
|
Provide Feedback