Search
5094 SERIAL
Troubleshooting
Internal error
Invalid character
Invalid data format combination
Invalid pad character value
Invalid start delimiter value
Invalid receive termination delimiter value
Invalid transmit termination delimiter value
Invalid termination delimiter 1 value
Invalid termination delimiter 2 value
Invalid value
Response Timer must be greater than Inter-Frame Timeout
Value is over range
Value is under range
Modbus data size is exceeded
Data index values are overlapping
Register start address values are overlapping
Provide Feedback
Have questions or feedback about this documentation? Please
submit your feedback here
.
Normal