Overview view

The 5094-SERIAL device provides communication connections to serial devices.
The device has two channels that are independent of each other. In the
Device definition
dialog box, use the
Overview
view to configure device definition parameters and to specify the protocol for each channel.
TIP:
If the channel is not used, set
Channel
to
Disabled
. If
Channel
is set to
Modbus Master
or
Modbus Slave
, use the
Channel
X
views in the
Device definition
dialog box to set up the Modbus Master and Modbus Slave.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal