Channel X view
Use the
Channel
view to configure the serial protocol for the channel.X
Use the
Channel
view to:X
- Set theBaud Rate,Data Bits,Parity, andStop Bits.
- Select whether the serial media isRS-232C,RS-422, orRS-485.
- Select theDuplexfor the serial media.
- Specify the delay between the time the RTS signal changes from low to high and the time data is sent.
- Specify the delay between the time the last character is sent and the time the RTS signal changes from high to low.
- View the Data Carrier Detect (DCD) wait delay time.
Provide Feedback