Channel X - Generic ASCII Receive view

Use the
Channel
X
- Generic ASCII Receive
view to define the data received from the serial device:
  • Select the swapping mode for data received from the serial port.
  • Select the handshake mode used to pass received data from the serial port to the controller.
  • Enter the message receive timeout value.
  • Specify the pad character used to fill the receive buffer when it is not full.
  • Select the start and termination mode.
  • Specify the start and termination delimiters.
  • Enable or disable the
    XON/XOFF
    flow control.
  • Determine whether
    Echo Mode
    is enabled or disabled.
  • Enter the maximum buffer length.
  • Select the
    Delete Mode
    .
  • Open the diagnostic dialog box to diagnose a communication problem with the Generic ASCII Receive /Transmit communication.
The
Generic ASCII Receive
view is available when
Channel
X
in the
Device definition
dialog box is set to
Generic ASCII
.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal