Configure counter parameters
Use the
Counters
view to view and configure counter parameters for the 5069-HSC2XOB4 high-speed counter device.
TIP:
Parameters not editable in the
Counters
view can be configured using device output tag members.To configure counter parameters
- On the tab for the device, selectCounters.
- In theCountersview, fill in the parameters and selectOK.
Provide Feedback