Ptxx Diagnostics parameters
Ptxx Diagnostics
includes these parameters:Parameter | Description | Value |
|---|---|---|
Field power | Shows whether field power is present on the point. |
|
Field power on timestamp | Shows the timestamp of the last time field power turned on in YYYY-MM-DD-HH:mm:SS_mmm (UTC-00:00) format.
| A valid time or None if there is no recorded event time. |
Field power off timestamp | Shows the timestamp of the last time field power turned off in YYYY-MM-DD-HH:mm:SS_mmm (UTC-00:00) format.
| A valid time or None if there is no recorded event time. |
Provide Feedback