Limits view parameters

The
Limits
view include these parameters:
Parameter
Description
High Clamp
Indicates the maximum value the output can take within the process with a range from -1.0E11...+1.0E11. The default value is 100% for Current mode. The value must be greater than the Low Clamp value. If an output above the high limit is requested, the HLimit alarm is set and the output signal remains at the configured high limit.
Low Clamp
Indicates the minimum value the output can take within the process with a range from -1.0E11...+1.0E11. The default value is 0. The value must be less than the High Clamp value. If an output below the low limit is requested, the LLimit alarm is set and the output signal remains at the configured low limit.
Disable All Alarms
Disables all alarms when the alarms will not be used.
Latch Clamp Alarms
Allows the latch clamp alarm to remain latched. This can be useful if alarm conditions need to be acknowledged by an operator.
Ramp in Run Mode
Enables output ramping during Run Mode. Output changes will be limited to the maximum ramp rate during Run Mode.
Latch Rate Alarm
Allows the latch Rate Alarm to remain latched. This can be useful if alarm conditions need to be acknowledged by an operator.
Ramp to Program Mode
Enables output ramping when transitioning to Program Mode or Inhibit mode. Output changes will be limited to the maximum ramp rate when transitioning to the program value.
Ramp to Fault Mode and Final Fault State
Enables output ramping when transitioning to either fault mode or final fault state. Output changes are limited to the maximum ramp rate when transitioning to the fault value or to the fault final state.
Ramp Rate
Defines the maximum rate at which the output is allowed to transition in Engineering Units/sec. This should be a non-negative value.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal