CJ Channels view parameters
The
CJ Channels
view includes these parameters:Parameter | Description |
|---|---|
Use RTB CJC | Determines whether it is required to use RTB CJC:
IMPORTANT:
This setting only takes effect when
the input type is Thermocouple, Disable Compensation is not set and Remote Cold
Junction Channel is not selected.
|
Cold Junction Channel | Displays the channel numbers that can be configured. If the channel Input Type is Thermocouple and Sensor Type is other than mV, the
CJChxx row gets enabled. Otherwise, this row is disabled. |
Disable Compensation | Determines whether cold junction compensation for the channel is disabled. If the checkbox is selected, the rest of the row is disabled. |
Sensor Offset | Offset added directly to the measured CJ temperature. Used to compensate for cold
junction temperature sensor error. |
Remote Cold Junction Channel | Determines which main channel to be used as a remote cold junction channel for
this channel.
|
Diagnostics | Accesses the Diagnostics dialog, which contains diagnostics information for the
channel. |
Provide Feedback