Revert to Factory Calibration view parameters
Parameter | Description |
|---|---|
Channel | Displays the channel number to which you can revert the current
calibration values. |
Revert to Factory Calibration | Defines which channel calibration values to be reverted to
factory calibrated vaules. |
Calibration Range | Displays the value currently configured for the channel. Values
display according to the Input Type selected. |
Current Calibration Gain | Displays the current calibration gain values reported by the
module. |
Current Calibration Offset | Displays the current offset in signal units reported by the
device. |
Calibration Status | Displays the status of the calibration for each channel. |
Provide Feedback