Channelxx Diagnostics dialog parameters (Input Modules)
The
Channelxx Diagnostics
dialog includes these parameters:
Parameter | Description |
|---|---|
Fault Exist | Displays whether a fault is present on the channel. |
Data Uncertain | Displays the module is operating outside the designed operating
range, or data is under manual or override control. |
Field Power | Displays whether field power is present on the channel. |
Open Wire Fault | Displays whether an Open Wire fault is present on the
channel. |
Overrange Fault | Displays whether a signal overrange fault is present on the
channel. |
Underrange Fault | Displays whether a signal underrange fault is present on the
channel. |
Range | If a connection is open, it displays the currently configured
range. If a connection is not open, it displays the most recently
configured range. |
Gain | Displays the channel calibration gain from the last valid
calibration. |
Offset | Displays the channel calibration offset from the last valid
calibration. |
Field Power On Timestamp | Displays the timestamp of the last time the field power turned on
in YYYY-MM-DD-HH:mm:SS.mmm format.
You can see a valid time or None if no event time was
recorded. |
Field Power Off Timestamp | Displays the timestamp of the last time the field power turned
off in YYYY-MM-DD-HH:mm:SS.mmm format.
You can see a valid time or None if no event time was
recorded. |
Open Wire Fault Timestamp | Displays the timestamp of the last Open Wire fault in
YYYY-MM-DD-HH:mm:SS.mmm format.
You can see a valid time or None if no event time was
recorded. |
Overrange Fault Timestamp | Displays the timestamp of the last Overrange fault in
YYYY-MM-DD-HH:mm:SS.mmm format.
You can see a valid time or None if no event time was
recorded. |
Underrange Fault Timestamp | Displays the timestamp of the last Underrange fault in
YYYY-MM-DD-HH:mm:SS.mmm format.
You can see a valid time or None if no event time was
recorded. |
Calibration Timestamp | Displays the timestamp of the last calibration in
YYYY-MM-DD-HH:mm:SS.mmm format.
You can see a valid time or None if no event time was
recorded. |
Provide Feedback