Servers view
Use
Servers
to enable and disable the TCP and UDP ports that are used by the device
when it acts as a server. EtherNet/IP uses TCP/IP or UDP/IP for communication.If the device profile is online to a configurable TCP or UDP server, use the settings
to:
- Enable or disable the port.
- View information about the TCP or UDP port.
- Refresh communication to obtain the latest port information from the device.
TIP:
The information in
Servers
is only
available when the project is online and configurable ports are available.Provide Feedback